InvenSense Enters Mass Production With The World’s First And Only Seven-Axis Motion Sensor

ICM-20789 enables Prosumer level flight control stability for Toy and Smart drones
SAN JOSE, Calif.--(BUSINESS WIRE)--Jan. 4, 2017-- InvenSense, Inc. (NYSE:INVN), a leading provider of MEMS sensors platform solutions, has entered mass production with the world’s only 7-axis motion sensor. The ICM-20789 integrates InvenSense’s leading 6-axis (3-axis accelerometer + 3-axis gyroscope) MEMS motion sensor with InvenSense’s world class pressure sensor, providing a solution with performance on par with best in class discrete parts. InvenSense six-axis motion sensors have long enabled the drone market, including toy and commercial segments, owing to their reliable core performance, and immunity to the wide range of harsh stimulus that a drone experiences in its various stages of flight. The ICM-20789 provides an easy upgrade path for our customers to build on the time-tested performance of InvenSense 6-axis sensors, by adding a relative pressure sensor based on capacitive technology with class leading performance and exceptional temperature stability. The combined performance in these two key areas are a must-have in toy drones, where a majority of consumers have limited flight control expertise, or smart drones that need to maintain autonomous flight stability, for example, in order to follow a user while capturing video.
The prosumer drone market has long been taking advantage of pressure sensors to ease flight take-off and landing, as well as provide stable hover mode using discrete six-axis and pressure sensors. The ICM-20789, complemented with InvenSense’ drone fusion software, specifically developed for this market, brings prosumer drone level stability to toy and smart drone markets. With accurate elevation control, a toy drone no longer need crash into ceilings indoors, end up on the roof, or trees outdoors as it will safely return to user’s hand to enjoy many more flights.
InvenSense ICM-20789 is in production with select customers now and will be available for wide distribution in Q2’2017. InvenSense is exhibiting in booth #31420 in South Hall 3 at the 2017 Consumer Electronics Show taking place in Las Vegas, Nevada from January 5 - 8, 2017. To schedule press and partner meetings at the show, contact pr@invensense.com. For additional information about the InvenSense ICM-20789, please visit www.invensense.tdk.com or contact InvenSense Sales at sales@invensense.com.
About InvenSense
InvenSense, Inc. (NYSE: INVN) is the world’s leading provider of MEMS sensor platforms. InvenSense’s vision of Sensing Everything™ targets the consumer electronics and industrial markets with integrated Motion and Sound solutions. Our solutions combine MEMS (micro electrical mechanical systems) sensors, such as accelerometers, gyroscopes, compasses, and microphones with proprietary algorithms and firmware that intelligently process, synthesize, and calibrate the output of sensors, maximizing performance and accuracy. InvenSense’s motion tracking, audio and location platforms, and services can be found in Mobile, Wearables, Smart Home, Industrial, Automotive, and IoT products. InvenSense is headquartered in San Jose, Californiaand has offices worldwide. For more information, go to www.invensense.tdk.com and http://www.coursaretail.com.
©2017 InvenSense, Inc. All rights reserved. InvenSense, Sensing Everything, FireFly, SensorStudio, TrustedSensor, Coursa, Coursa Sports, Coursa Retail, UltraPrint, MotionTracking, MotionProcessing, MotionProcessor, MotionFusion, MotionApps, InvenSenseTV, DMP, AAR, and the InvenSense logo are trademarks of InvenSense, Inc. Other company and product names may be trademarks of the respective companies with which they are associated.
View source version on businesswire.com: http://www.businesswire.com/news/home/20170104005543/en/
Source: InvenSense, Inc.
Contacts for regional media
No media contacts available
Upcoming events: Start date